Everything
3.2.8 Total Section Size

The total sizes of ROM, RAM, and program sections are output. The following figure shows an example of total section size output.

*** Total Section Size ***
RAMDATA SECTION :       00000660 Byte(s)  (1)
ROMDATA SECTION :       00000174 Byte(s)  (2)
PROGRAM SECTION :       000016d6 Byte(s)  (3)

Item Number

Description

(1)

Total size of RAM data sections

(2)

Total size of ROM data sections

(3)

Total size of program sections