Everything
3.2.9 Vector Information

The contents of the variable vector table are output when -show=vector is specified. The following figure shows an example of vector information output.

*** Variable Vector Table List ***
(1)     (2)
NO.     SYMBOL/ADDRESS
 0      $fdummy
 1      $fa
 2      00ff8800
 3      $fdummy
   :
<Omitted>

Item Number

Description

(1)

Vector number

(2)

Symbol. When no symbol is defined for the vector number, the address is output.