Calculates the positive square root of a floating-point number.
[Format]
#include <math.h>
double sqrt (double d);
float sqrtf (float d);
long double sqrtl (long double d);
[Parameters]
d Floating-point number for which positive square root is to be computed
[Return values]
Normal: Positive square root of d
Abnormal: Domain error: Returns not-a-number.
[Remarks]
A domain error occurs if d is negative.