2.2.1.1
[Full-spec emulator]
Connect a host machine and Full-spec emulator. If required, connect a target board, too.
For details on the connection method, see the user's manual for Full-spec emulator.
Figure 2.1 | Connection Example [Full-spec emulator] |