Connect a host machine and E1. If required, connect a target board, too.
For details on the connection method, see the user's manual for E1.
Figure 2.2 | Connection Example [E1] |
Caution 1. | Only the Low Pin Debug interface (hereafter referred to as LPD communications) is supported for communication with the target board. |
Caution 2. | For details on the connection using a debug MCU board, see the user's manual for debug MCU board. |