Everything
2.2.1.3 [E20]

Connect a host machine and E20. If required, connect a target board, too.

For details on the connection method, see the user's manual for E20.

Figure 2.3

Connection Example [E20]

Caution 1.

Only the Low Pin Debug interface (hereafter referred to as LPD communications) is supported for communication with the target board.

Caution 2.

For details on the connection using a debug MCU board, see the user's manual for debug MCU board.