Clicking the following buttons jumps to each panel which selected events address exist.
Note however, that when a Trace event/Timer Result event/Performance Measurement event/Unconditional Trace event/Run-Break Timer event is selected, these buttons are disabled.
Opens the Editor panel and jumps to the source line corresponding to the address where the selected event is being set. |
|
Opens the Disassemble panel and jumps to the disassemble results corresponding to the address where the selected event is being set. |
|
Opens the Memory panel and jumps to the source line corresponding to the address where the selected event is being set. |