To delete any event and event condition you have set, select the event and click the 
 button on the toolbar. 
Note that it is not possible to delete the built-in events (Unconditional Trace event and Run-Break Timer event).
For the Break event of execution type, it is possible to delete the set event to click the event mark displayed in the Editor panel/Disassemble panel.  | 
 button (note, however, that it is not possible to delete the built-in events).