Everything
2.19.4.2 Edit access-related events

The address condition, data condition and pass count condition [Simulator] for access-related events you have set can be edited.

Perform this operation in the Detail dialog box (for access events) that is opened by selecting [Edit Condition...] from the context menu after moving the caret to an access-related eventNote you want to edit on the Events panel.

Note

An access-related event refers to any one of the following events in the Events panel.

-

Hardware Break event (access type)

-

Access-related event as start and end condition in detailed information on Trace event

-

Access-related event in detailed information on Point Trace event

-

Access-related event as start and end condition in detailed information on Performance Measurement event

For the access-related events that were set according to the descriptions in 2.11.5.1 Set a break event (access type), 2.14.3.1 Set a Trace event, 2.14.4.1 Set a Point Trace event, and 2.16.1.1 Set a Performance Measurement event the initial values of the address, data, and pass count conditions are listed below.

Table 2.25

Initial Values of Address Conditions

Item

Initial Value

Hardware Break

Trace,

Point Trace,

Performance Measurement

Compare condition

[Full-spec emulator][E1][E20]

RH850G3M, RH850G3K, RH850G3MH, RH850G3KH:

Specified address (==)

RH850G4MH:

When a value for comparison has been specified:

Inside the range (<=Addresses<=)

When a value for comparison has not been specified:

Specified address (==)

GTM:

Inside the range (<=Addresses<=)

[Simulator]

Specified address (==)

[Full-spec emulator][E1][E20]

Inside the range (<=Addresses<=)

[Simulator]

Specified address (==)

Address

Address at the time of setting the event

Start address

Address at the time of setting the event

End address

Address at the time of setting the event

Use the address mask

No

Mask value

0xFFFFFFFF

Table 2.26

Initial Values of Data Conditions

Item

Initial Value

Access type

Access type at the time of setting the event

Access size

Variable or I/O register size at the time of setting the event

Compare condition

When a value for comparison has been specified : Specified value (==)

When a value for comparison has not been specified : No conditions

Data

Data at the time of setting the event

Lower data

Data at the time of setting the event

Upper data

Data at the time of setting the event

Use the data mask

No

Mask value

0xFFFFFFFF

Table 2.27

Initial Values of Pass count Conditions

Item

Initial Value

Pass count [Simulator]

1