This dialog box is used to display and modify detailed information on an access-related event selected in the Events panel.
This section describes the following.
On the Events panel, move the caret to any one of the following events, and then select [Edit Condition...] from the context menu.  | 
Access-related event as start and end condition in detailed information on Performance Measurement event  | 
Specify the address condition.
| 
 Specify the condition to compare address. The condition for an access event being generated varies with the value of this setting. : Before Read, Before Write, Before Read/Write [Inside the range (<=Addresses<=)] / [Outside the range !(<=Addresses<=)]  | 
||||
| 
 Specifies the address with [Address].  | 
||||
| 
 Specifies the range with [Start address] and [End address].  | 
||||
| 
 This item appears only when [Specified address (==)], [Greater than or equal to (>=)] or [Less than or equal to (<=)] is selected in [Compare condition].  | 
||||
| 
 This item appears only when [Inside the range (<=Addresses<=)] or [Outside the range !(<=Addresses<=)] is selected in [Compare condition].  | 
||||
| 
 This item appears only when [Inside the range (<=Addresses<=)] or [Outside the range !(<=Addresses<=)] is selected in [Compare condition].  | 
||||
| 
 Specify whether to specify an address mask. This item appears only when [Specified address (==)] is selected in [Compare condition].  | 
||||
| 
 Specify the value of address mask. This item appears only when [Use the address mask] is set to [Yes].  | 
||||
| 
 In [Compare condition] under [[Data Condition]], only [No conditions] is selectable.  | 
||||
| 
 Sets 16-byte as the access size. In [Compare condition] under [[Data Condition]], only [No conditions] is selectable. This item only appears when the selected microcontroller supports it.  | 
||||
| 
 Specify the condition to compare the data. This item appears only when [1byte], [2byte], [4byte] or [8byte] is selected in [Access size].  | 
||||
| 
 Specifies the data with [Data].  | 
||||
| 
 Specifies the range with [Lower data] and [Upper data].  | 
||||
| 
 This item appears only when [Specified value (==)], [Any other value (!=)], [Greater than or equal to (>=)] or [Less than or equal to (<=)] is selected in [Compare condition].  | 
||||
| 
 Hexadecimal number up to [Access size]  | 
||||
| 
 Specify the lower data for the range in [Compare condition]. This item appears only when [Inside the range (<=Values<=)] or [Outside the range !(<=Values<=)] is selected in [Compare condition].  | 
||||
| 
 Hexadecimal number up to [Access size]  | 
||||
| 
 Specify the upper data for the range in [Compare condition]. This item appears only when [Inside the range (<=Values<=)] or [Outside the range !(<=Values<=)] is selected in [Compare condition].  | 
||||
| 
 Hexadecimal number up to [Access size]  | 
||||
| 
 Specify whether to specify a data mask. This item appears only when [1byte], [2byte], [4byte] or [8byte] is selected in [Access size]. This item appears only when [Specified value (==)] or [Any other value (!=)] is selected in [Compare condition].  | 
||||
| 
 Specify the value of data mask. This item appears only when [Use the data mask] is set to [Yes].  | 
||||
| 
 Hexadecimal number up to [Access size]  | 
||||
Specify the pass count condition.
| 
 The relevant event occurs when the event condition is met as many times as the specified pass count.  | 
||||
This area displays a simple description of the item selected in the Event conditions setting area.
| 
 Displays all categories in the Event conditions setting area.  | 
||
| 
 Hides categories in the Event conditions setting area and rearranges only setting items in the ascending order  | 
||