Everything
 

Bookmarks dialog box


This dialog box is used to display the position where a bookmark is to be set or to delete a bookmark.

Figure A.15

Bookmarks Dialog Box

 

The following items are explained here.

[How to open]

-

Click the button on the bookmark toolbar.

-

From the [Edit] menu, select [Bookmark] >> [List Bookmarks...].

-

On the Editor panel, select [Bookmark] >> [List Bookmarks...] from the context menu.

[Description of each area]

(1)

Bookmark list area

This area displays a list of bookmarks that have been registered.

The bookmarks are listed alphabetically by file name for [Bookmark]. Bookmarks in the same file are listed in line number order.

When a bookmark is added to the Editor panel, a bookmark function is added.

In the bookmark list area, double-clicking on a line moves a caret to the corresponding position for the bookmark.

(a)

[File]

Displays the name of the file (without any path) in which a bookmark is registered.

(b)

[Line Number]

Displays the number of the line to which the bookmark is registered.

(c)

[Path]

Displays the path of the file in which the bookmark is registered.

(d)

Buttons

View

Moves a caret to the selected position for the bookmark.

However, this button is disabled when no bookmark is selected, two or more bookmarks are selected, or no bookmark is registered.

Remove

Removes a selected bookmark. When two or more bookmarks are selected, all of those selected are removed.

However, this button is disabled when no bookmark is selected or no bookmark is registered.

Remove All

Removes all the registered bookmarks.

This button is disabled when no bookmark is registered.

Caution

Registered bookmarks are not deleted even if the Editor panel is closed.
Note, however, that if the Editor panel in which a file that has never been saved is being displayed is closed, then registered bookmarks will be deleted.

[Function buttons]

Button

Function

Previous

Moves a caret to the position of the bookmark previous to the selected bookmark.

This button is disabled in the following cases.

-

A bookmark shown in the first line has been selected.

-

No bookmark is selected.

-

Two or more bookmarks are selected.

-

No bookmark is registered.

-

Only one bookmark is registered.

Next

Moves a caret to the position of the bookmark next to the selected bookmark.

This button is disabled in the following cases.

-

A bookmark shown in the last line has been selected.

-

No bookmark is selected.

-

Two or more bookmarks are selected.

-

No bookmark is registered.

-

Only one bookmark is registered.

Close

Closes this dialog box.

Help

Displays the help for this dialog box.