Everything
A.1 Description

Windows/panels/dialog boxes used with the editor features are listed below.

Table A.1

Window/Panel/Dialog Box List

Window/Panel/Dialog Box Name

Description

Editor panel

Enables text files to be viewed and edited, and is used to execute source level debug.

Encoding dialog box

Selects a file-encoding.

Save Settings dialog box

Specifies the encoding and the new line code of the file being edited.

Find and Replace dialog box

Finds and replaces the designated characters.

Go to Line dialog box

Moves the caret to the specified line.

Jump to Function dialog box

Selects a function to which the caret moves.

Bookmarks dialog box

Displays and deletes bookmarks.

Print Preview window

Previews the source file before printing.