Everything
2.2.3 Add column

The Pin Configurator is used to add the "user's own column" to the device pin list using the [New Column...] button in the Column Chooser dialog box that opens by pressing the button in the upper left corner of the device pin list.

To add a column, use the New Column dialog box that opens by pressing the [New Column...] button in the Column Chooser dialog box.

Figure 2.4

Add Column

 

Remark

On the device pin list, adding columns to the first level of [Macro] tab, [External Peripheral] tab is restricted.