Everything
2.2.1 Select item

The Pin Configurator is used to select items to be displayed in the device pin list using the button in the upper left corner of the device pin list.

To select the item to be displayed, use the Column Chooser dialog box that opens by pressing the button in the upper left corner of the device pin list.

Figure 2.2

Select Item

 

Remark

To select the item to be displayed, check the check box that corresponds to the item.

Checked

Displays the selected item in the device pin list.

Not checked

Hides the selected item in the device pin list.