This panel displays components of the project (microcontroller, design tool, build tool, etc.) in a tree structure.
The following items are explained here.
This area displays components of the project (microcontroller, design tool, build tool, etc.) in a tree structure.
This node consists of the following pin nodes.
Opens the Device Pin List panel for entering information on the pins of the microcontroller. |
|
Opens the Device Top View panel that displays the information entered in the Device Pin List panel. |
Opens the Property panel corresponding to the selected node. |