Everything

DownloadInfo


This class holds download information (return value of the debugger.Download.Information function).

[Type]

class DownloadInfo:
        Number = None
        Name = None
        ObjectDownload = True
        SymbolDownload = False

[Variable]

Variable

Description

Number

This holds the download number.

Name

This holds the file name.

ObjectDownload

This holds whether object information has been downloaded or not.

True: Object information has been downloaded.

False: Object information has not been downloaded.

SymbolDownload

This holds whether symbol information has been downloaded or not.

True: Symbol information has been downloaded.

False: Symbol information has not been downloaded.

[Detailed description]

-

DownloadInfo is a class, and it is the structure of the return value from the debugger.Download.Information function.

[Example of use]

>>>info = debugger.Download.Information()
   1: DefaultBuild\sample.out
>>>print info[0].Number
1
>>>print info[0].Name
DefaultBuild\sample.out
>>>print info[0].ObjectDownload
True
>>>print info[0].SymbolDownload
True
>>>