Everything

StackInfo


This class holds stack information (return value of the debugger.Where function).

[Type]

class StackInfo:
        Number = 0
        AddressInfoText = None

[Variable]

Variable

Description

Number

This holds the stack number.

AddressInfoText

This holds the stack address information as a string.

[Detailed description]

-

StackInfo is a class, and it is the structure of the return value from the debugger.Where function.

[Example of use]

>>>info = debugger.Where()
   1: test2.c#
   2: test1.c#main#41
>>>print info[0].Number
1
>>>print info[0].AddressInfoText
test2.c#
>>>info = debugger.Where
1: test2.c#
--- Information below might be inaccurate.
2: test1.c#main#41
>>>print a[1].Number
None
>>>print a[1].AddressInfoText
--- Information below might be inaccurate.
>>>