Everything

BreakCondition


This class creates a break condition.

[Type]

class BreakCondition:
        Address = ""
        Data = None
        AccessSize = None
        BreakType = BreakType.Hardware

[Variable]

Variable

Description

Address

Specify the address at which to set a break.

Must be specified.

Data

Specify the number to set as a break condition for the data.

If "None" is specified, then the data condition is ignored.

AccessSize

Specify the access size (8, 16, 32, or 64).

If "None" is specified, then all access sizes will be specified.

BreakType

Specify the break type.

The break types that can be specified are shown below.

Type

Description

BreakType.Software

Software break (except a simulator)

BreakType.Hardware

Hardware break (default)

BreakType.Read

Data read break

BreakType.Write

Data write break

BreakType.Access

Data access break

[Detailed description]

-

"BreakCondition" is in class format, and the break condition is set in the variable.
In order to create a break condition, create an instance, and set conditions for that instance.

[Example of use]

>>>executeBreak = BreakCondition()          ... Create instance
>>>executeBreak.Address = "main"
>>>executeBreak.BreakType = BreakType.Software
>>>debugger.Breakpoint.Set(executeBreak)    ... Specify function in which to set the break point in parameter
>>>
>>>dataBreak = BreakCondition()             ... Create instance
>>>dataBreak.Address = "chData"
>>>dataBreak.Data = 0x10
>>>dataBreak.BreakType = BreakType.Access
>>>debugger.Breakpoint.Set(dataBreak)       ... Specify function in which to set the break point in parameter
>>>
>>>executeBreak.Address = "sub + 0x10"      ... Reuse break condition
>>>debugger.Breakpoint.Set(executeBreak)    ... Specify function in which to set the break point in parameter
>>>