Everything

project.Change


This function changes the active project.

[Specification format]

project.Change(projectName)

[Argument(s)]

Argument

Description

projectName

Specify the full path of the project or subproject to be changed.

[Return value]

If the active project was changed successfully: True

If there was an error when changing the active project: False

[Detailed description]

-

This function changes the project specified in projectName to the active project.

-

The project file specified in projectName must be included the currently opened project.

[Example of use]

>>>project.Close("C:/project/sample/sub1/subproject.mtpj")
True
>>>