Below is a list of CS+ Python functions (for a project).
Table B.3
CS+ Python Function (For Project)
Function Name
Function Description
project.Change
This function changes the active project.
project.Close
This function closes a project.
project.Create
This function creates a new project.
project.File.Add
This function adds a file to the active project.
project.File.Exists
This function confirms whether the file exists in the active project.
project.File.Information
This function displays the list of the files registered in the active project.
project.File.Remove
This function removes a file from the active project.
project.GetDeviceNameList
This function displays the list of the device names of the microcontroller.
project.GetFunctionList
This function displays the list of the functions of the active project.
project.GetVariableList
This function displays the list of the variables of the active project.
project.Information
This function displays the list of project files.
project.Open
This function opens a project.