Everything

project.GetVariableList


This function displays the list of the variables of the active project.

[Specification format]

project.GetVariableList(fileName = "")

[Argument(s)]

Argument

Description

fileName

Specify the full path of the file that the list of the variables are displayed (default: not specified).

[Return value]

List of variable information (see the VariableInfo property for detail)

[Detailed description]

-

This function displays the list of the variables of the active project shown by the following format.

variable-name attribute type address size file-name

-

When fileName is specified, only the variables included in the specified file are displayed.

-

When fileName is not specified, then all the variables will be displayed.

Caution

This function uses the information displayed in the list of variables for program analysis.

[Example of use]

>>>project.GetVariableList()
var1 volatile int 0x000014e4 4 C:\project\src\test1.c
var2 static int 0x000014e8 4 C:\project\src\test2.c
>>>project.GetVariableList("C:/project/src/test1.c")
var1 volatile int 0x000014e4 4 C:\project\src\test1.c
>>>