RS-CAN Module Setting dialog box [Full-spec emulator][E1][E20] |
This dialog box is used to make settings related to the entire RS-CAN module shown in the Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20].

This section describes the following.
On the Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20], click the [RS-CAN Module Setting...] button on the toolbar. |
Select the clock source for the RS-CAN module from the following drop-down list.
The actual frequency of the specified clock source appears at the bottom of the drop-down list.
Specify whether the timestamp function of the RS-CAN is to be used.
Specify whether the Data Length Code (DLC) checking function of the RS-CAN is to be used.
Specify whether the DLC replacement function of the RS-CAN is to be used.
This item is specifiable only when the DLC checking function is used.
Reflects the clock source, timestamp, DLC checking function, and DLC replacement function settings that were made in this dialog box to the [RS-CAN settings] area on the Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20]. |
|