This panel is central to the functionality of the solution for pseudo-error debugging.
See "2.24 Pseudo-error Debugging [Full-spec emulator][E1][E20]" for details on the solution for pseudo-error debugging.
This section describes the following.
This area lists pseudo-errors which are targets in pseudo-error debugging.
The full name of a pseudo-error is displayed by hovering the mouse cursor over the node of each pseudo-error.
Each item is explained as follows:
When a check box is selected, this pseudo-error is generated after pseudo-error debugging starts.
This column shows whether this pseudo-error has been generated when the debugger is stopped.
"!" is displayed if the pseudo-error has been generated and nothing is displayed if it has not been generated.
A bit is always assigned per error to indicate whether an error occurred. Two bits are assigned to some errors and the number of occurrences of an error that can be counted is up to three (e.g., this is the case for errors No. 0 to 7 in RH850/G4MH devices). If the pseudo-error has occurred several times, “!” will be displayed as the number of times the error has occurred. To check the number of bits that are assigned to an error, see “ECM Error Source Status Register” in the chapter of the ECM in User's Manual: Hardware for the MCU in use.  | 
The abbreviated name of this pseudo-error is displayed.
The bit name of IOR that triggers the generation of this pseudo-error is displayed.
A list of breakpoints that are to be used for pseudo-error debugging is displayed.
Only the breakpoints whose check box is selected will be valid for pseudo-error debugging.
Either of the following icons is displayed at the beginning of each breakpoint.
| 
 Starts pseudo-error debugging based on the settings made in this panel.  | 
|
| 
 Has the same functionality as the same button on the Debug toolbar in the Main window.  | 
|
| 
 Opens the Select Pseudo-Error dialog box [Full-spec emulator][E1][E20] used to select ECM pseudo-errors that are targets of pseudo-error debugging.  | 
|
| 
 Opens the Breakpoint Setting dialog box [Full-spec emulator][E1][E20] to add a breakpoint.  | 
|