This panel shows the constituent elements of the project (e.g., microcontroller, build tool, and debug tool) in tree form.
Note that the debug tools used are selected or switched from one to another on this panel.
This section describes the following.
This area displays the project's constituent elements in tree form at the following nodes.
When a node is selected, its detailed information (properties) is displayed on the Property panel allowing the settings on it to be changed. (If this panel is not open yet, double-click a node to open it.)
|
Shows a cascaded menu to select the debug tool used. Note that the debug tools displayed here differ with the microcontroller type selected for the project (see "Table 2.1 Relationship between Types of Microcontroller and Connectable Debug Tools"). |
||
|
Displays the properties of the selected debug tool on the Property panel. |
||