The table below lists the windows, panels and dialog boxes associated with debugging.
|
Displays detailed information on a debug tool selected on the Project Tree panel and changes settings. |
|
|
Displays disassembled result of memory values and performs line assembly and instruction-level debugging. |
|
|
Displays contents of CPU registers (program and system registers) and changes values. |
|
|
Displays contents of registered watch-expressions and changes values. |
|
|
Displays detailed information on set events, chooses to enable or disable events, and deletes events. |
|
|
Displays messages output by the build tool, debug tool or each plug-in, or displays result of global search performed in Find and Replace dialog box. |
|
|
Selects a file to be downloaded and sets download condition. |
|
|
Sets the number of view columns of memory values on the Memory panel. |
|
|
Sets an offset value for the address display on the Memory panel. |
|
|
Sets a print range on the Disassemble panel. |
|
|
Displays the conditions for event combination and modifies the settings. |
|
|
Detailed Settings of Timer Measurement dialog box [E1] [E20] |
Displays the detailed information on timer events and modifies the settings. |
|
Displays the detailed information on execution-related events and modifies the settings. |
|
|
Displays the detailed information on access-related events and modifies the settings. |
|
|
Detailed Settings of Interrupt Events dialog box [Simulator] |
Displays the detailed information on interrupt events and modifies the settings. |
|
Sets COM port in the Debug Console panel. |
|
|
Sets a scroll range on the Memory panel/Disassemble panel. |
|
|
Displays the functions that access variables in the form of an orthogonal table. |
|
|
This panel is central to the functionality of the solution for measuring current consumption. |
|
|
Current Consumption Measurement Condition Setting dialog box [E2] |
This dialog box is used to set measurement conditions in the Measuring Current Consumption panel [E2]. |
|
Current Consumption Measurement Trigger Condition Setting dialog box [E2] |
This dialog box is used to set trigger conditions in the Measuring Current Consumption panel [E2]. |
|
This dialog box is used to specify and search the detailed conditions in the Measuring Current Consumption panel [E2]. |
|
|
This dialog box is used to save the values for current in the Measuring Current Consumption panel [E2]. |