This dialog box is used to set the plug-ins to be read in when this product is started.

The following items are explained here.
By selecting a tab, the plug-ins displayed in the plug-in list area are switched.
This dialog box has the following tabs:
Select the plug-ins read when this product is started with check boxes.
For details of displayed items/setting method, see the description of each tab.
You can select all check boxes or clear them by clicking buttons displayed on the upper left of this area. |