This panel is used to display the message that is output from the build tool/debug tool/each plug-in or the result of the Find In Files with the Find and Replace dialog box.
Messages are shown individually on the tab categorized by the output tool.
The [All Messages] tab consolidates and displays all output messages.
This panel can be zoomed in and out by |

The following items are explained here.
Displays messages and the search results output from each tool.
The [All Messages] tab consolidates and displays all output messages.
The message colors differ as follows depends on the type of the output message (the character color/background color is set in the [General - Font and Color] category in the Option dialog box).
This area has the following functions.
When the output message is double-clicked, or the [Enter] key is pressed with the caret over the message, Editor panel appears and the destination line number of the file is displayed.
You can jump to the line of the source file that generated the error from the error message output when building.
When [Help for Message] in the context menu is selected or [F1] key is pressed while the caret is in the line where the warning message or the error message is displayed, the help with regard to the displayed message or the message at the current caret is displayed.
And a Web browser is displayed and a search for FAQs with regard to the message is started.
When [Online] is selected from [How to Access Help] and the [Search FAQ when the help of a message opens.] check box is selected, the help or FAQs may not be displayed. |
Use the offline help. (From the [Help] menu, select [How to Access Help] >> [Offline].)
Hide FAQs. (Clear the [Search FAQ when the help of a message opens.] check box in the [General - Smart Browser] category of the Option dialog box.)
FAQs can be searched on the Smart Browser panel. Enter the message number, etc. in the text box and click the [Search FAQ] button.
The contents displayed on the currently selected tab can be saved in a text file (*.txt) by selecting [Save Output - tab name As...] from [File] menu and opens the Save As dialog box (messages on the tab that is not selected will not be saved).
Select tabs that messages are output from.
Tabs that are displayed are as follows.
Tab is not automatically switched when a new message is output on the non-selected tab. |
[[File] menu (Output panel-dedicated items)]
The following items are exclusive for [File] menu in the Output panel (other items are common to all the panels).
Saves the contents on the currently selecting tab in the previously saved text file (*.txt) (see "(c) Save of log"). When this menu is selected for the first time after launching the program, the operation is equivalent to when selecting [Save tab name As...]. |
|
Opens the Save As dialog box to save the contents on the currently selecting tab in the designated text file (*.txt) (see "(c) Save of log"). Note that this operation is invalid while user program is executed. |
[[Edit] menu (Output panel-dedicated items)]
The following items are exclusive to [Edit] menu in the Output panel (other items are all invalid).
Opens the Find and Replace dialog box with the [Quick Find] tab target. |
|
Opens the Find and Replace dialog box with the [Replace in Files] tab target. |