Starts simple IIC master reception.
Remark This API function performs byte-level simple IIC master reception the number of times specified by the argument rx_num, and stores the data in the buffer specified by the argument rx_buf.
[Syntax]
#include “r_cg_macrodriver.h”
void R_IICmn_Master_Receive ( uint8_t adr, uint8_t * const rx_buf, uint16_t rx_num );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
|
I/O |
Argument |
Description |
|
I |
uint8_t adr; |
Device address |
|
O |
uint8_t * const rx_buf; |
Pointer to a buffer to store the received data |
|
I |
uint16_t rx_num; |
Total amount of data to receive |
Remark Below is shown the format for specifying device address adr.

[Return value]
None.