Starts simple IIC master transmission.
Remark This API function repeats the byte-level simple IIC master transmission from the buffer specified in argument tx_buf the number of times specified in argument tx_num.
[Syntax]
#include “r_cg_macrodriver.h”
void R_IICmn_Master_Send ( uint8_t adr, uint8_t * const tx_buf, uint16_t tx_num );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
|
I/O |
Argument |
Description |
|
I |
uint8_t adr; |
Device address |
|
I |
uint8_t * const tx_buf; |
Pointer to a buffer storing the transmission data |
|
I |
uint16_t tx_num; |
Total amount of data to send |
Remark Below is shown the format for specifying device address adr.

[Return value]
None.