Usage example
Use timer as One-shot timer.
[GUI setting example]
| 
       8bit interval timer  | 
    
       Used  | |||
| 
       IT8bit0  | 
    
       Used  | |||
| 
       Channel0  | 
    
       Used  | |||
| 
       Channel 0  | 
    
       8 bit  | |||
| 
       Interval timer operation setting  | 
    
       Auto  | |||
| 
       Interval value  | 
    
       100ms (Actual value:7.8125)  | |||
| 
       Detection of compare match (INTIT00)  | 
    
       Used  | |||
| 
       Priority  | 
    
       Low  | |||
[API setting example]
r_cg_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start 8 bit interval timer unit0 Channel0 operation */
R_IT8Bit0_Channel0_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}
r_cg_it8bit_user.c
static void __near r_it8bit0_channel0_interrupt(void)
{
/* Start user code. Do not edit comment generated here */
/* Stop 8 bit interval timer unit0 Channel0 operation */
R_IT8Bit0_Channel0_Stop();
/* End user code. Do not edit comment generated here */
}