Gets the result of conversion.
[Syntax]
#include "r_cg_s12ad.h"
void R_S12ADn_Get_ValueResult ( ad_channel_t channel, uint16_t * const buffer );
Remark n is the unit number.
[Argument(s)]
| I/O | Argument | Description | 
| I | ad_channel_t channel; | Channel number ADCHANNEL0 : Input channel AN000 ADCHANNEL1 : Input channel AN001 ADCHANNEL2 : Input channel AN002 ADCHANNEL3 : Input channel AN003 ADCHANNEL4 : Input channel AN004 ADCHANNEL5 : Input channel AN005 ADCHANNEL6 : Input channel AN006 ADCHANNEL7 : Input channel AN007 ADCHANNEL8 : Input channel AN008 ADCHANNEL9 : Input channel AN009 ADCHANNEL10 : Input channel AN010 ADCHANNEL11 : Input channel AN011 ADCHANNEL12 : Input channel AN012 ADCHANNEL13 : Input channel AN013 ADCHANNEL14 : Input channel AN014 ADCHANNEL15 : Input channel AN015 ADCHANNEL16 : Input channel AN016 ADCHANNEL17 : Input channel AN017 ADCHANNEL18 : Input channel AN018 ADCHANNEL19 : Input channel AN019 ADCHANNEL20 : Input channel AN020 ADTEMPSENSOR : Extended analog input (temperature sensor output) ADINTERREFVOLT : Extended analog input (internal reference voltage) | 
| O | uint16_t * const buffer; | Pointer to the area where the results of conversion are stored | 
[Return value]
None.