-   
 
   [RI78V4] tab
  
    -   
  
 
 This tab shows the detailed information on the RI78V4 to be used categorized by the following.
 
 1 )	 [Version Information]
 
 The detailed information on the version of the RI78V4 are displayed.
 
 
  
  
    | 
 | 
    
 Display the version of the RI78V4 to be used.
  
 Note that the version is set permanently when the project is created, and cannot be changed.
  
 | 
  
  
    | 
 | 
    
 | 
  
  
    | 
 | 
    
 | 
  
  
    | 
 | 
    
 Display the folder in which the RI78V4 to be used is installed with the absolute path.
  
 | 
  
  
    | 
 | 
    
 The folder in which the RI78V4 to be used is installed
  
 | 
  
  
    | 
 | 
    
 | 
  
  
    | 
 | 
    
 Display the memory model set in the project.
  
 Display the same value as the value of the [Memory model type] property of the build tool.
  
 | 
  
  
    | 
 | 
    
 The memory model selected in the property of the build tool
  
 | 
  
  
    | 
 | 
    
 |