This option output information messages.
[Specification format]
 
-  | Interpretation when omitted  | 
 
The output of information messages is suppressed (It is the same result as when the -nomessage option is specified).
[Detailed description]
-  | This option output information messages.  | 
 
[Example of use]
-  | To output information messages, describe as:  | 
 
>rlink a.obj b.obj -message 
 |