This option notifies the user of the external defined symbol that is not referenced.
[Specification format]
 
-  | Interpretation when omitted  | 
 
None
[Detailed description]
-  | This option notifies the user of the external defined symbol that is not referenced during link processing through an output message.  | 
 
[Example of use]
-  | To notify the user of the external defined symbol that is not referenced, describe as:  | 
 
>rlink a.obj b.obj -message -msg_unused 
 | 
 
[Remark]
-  | If a load module file is input, this option will be invalid.  | 
 
-  | This option must be specified together with the -message option.  | 
 
-  | The a message may be output for the function that inline expansion was performed during compilation. 
In this case, add a static declaration for the function definition to suppress the output of the message.  | 
 
-  | If there are references to constant symbols within the same file, references are not correctly analyzed so that information notified by the output messages will be incorrect.  |