Instructions are translated into machine language as a result of assembling, but directives are not converted into machine language in principle.
Directives contain the following functions mainly:
To provide the information required for assemblers and optimizing linkers to perform their intended processing |
The following table shows the types of directives.
|
.LINE, .STACK, ._LINE_TOP, ._LINE_END, .VECTOR, .ALIAS [V1.11.00 or later], .TYPE [V1.11.00 or later] |
|
The following sections explain the details of each directive.
In the description format of each directive, "[ ]" indicates that the parameter in square brackets may be omitted from specification, and "..." indicates the repetition of description in the same format.