< Optimizing Linkage Editor (rlink) Options / Output Options >
When this option is omitted, the default is form=absolute.
Table 2.14 lists the suboptions. |
|
Outputs an object file. This is specified when a module is extracted as an object file from a library with the extract option. |
||
|
When library=s is specified, a system library is output. |
||
|
Outputs a HEX file. For details of the HEX format, refer to HEX File Format. |
||
|
Outputs an S-type file. For details of the S-type format, refer to S-Type File Format. |
||
Table 2.15 shows relations between output formats and input files or other options.
message/nomessage, change_message, logo/nologo, form, list, and subcommand can always be specified. |
byte_count can be used only when form=hexadecimal or form=stype is specified for the output format. |