|
-create_unfilled_area [V2.03.00 or later]
|
< Optimizing Linkage Editor (rlink) Options / Output Options >
[Format]
[Description]
- | This option is available in V2.03 and later versions of this compiler. |
- | When a Motorola S-record file (<name>.mot) or Hex file (<name>.hex) is output, this option blocks spaces created by .OFFSET directives in the assembly language being filled with output data. |
- | When using this option, specify it when using the ccrx or asrx command to create an object file (<name>.obj) as well as when using the rlink command to create a Motorola S-record file or Hex file. |