2.1 Overview
 The resource information tool can be used to confirm the resource information (e.g. system information and memory area information) that changes dynamically as the program executes.
 Remarks 1.	 When a program using the RI78V4 functionality is downloaded, this panel opens automatically.
 2.	 The value will be indeterminate for the resource information shown when the RI78V4 system initialization is incomplete, because it will not be managed by the RI78V4.
 2.	 You can debug a program efficiently using “Section skip function” of the debugger. For example “step in” execute on a service call issue point, the debugger skip all internal process of RI78V4 and break by reaching the user application part. See "CS+ RL78 Debug" for details on "Section skip function".
 On the Realtime OS Resource Information panel tabs (e.g. [System] tab and [Memory Area] tab), check the current status of the resource information.