| 
 Specified Section dialog box 
 | 
This dialog box is used to specify the range for skipping step execution.
Figure A.53  | Specified Section Dialog Box  | 
 
 
This section describes the following. 
[How to open]
[Description of each area]
(1)  | [Specified section list] area   | 
 
This area is used to display the list of the range for skipping step execution.
To add a new section, click the [Add] button in this area, then in the [Specified section property] area, specify the sections to add.
| 
 | 
 | 
| 
 
Up 
 | 
 
Moves the selected section up one row in the list.  
Clicking this for the top section in the list has no effect. 
 | 
| 
 
Down  
 | 
 
Moves the selected section down one row in the list. 
Clicking this for the bottom section in the list has no effect. 
 | 
| 
 
Add 
 | 
 
Adds an empty item "-" to the list, and selects it.   
Specify the section to add in the [Specified section property] area.  
 | 
| 
 
Remove 
 | 
 
Removes the selected section from the list.  
 | 
 
(2)  | [Specified section property] area  | 
 
This area is used to display or edit the section selected in the [Specified section list] area. 
It can also be used to specify the new sections added via the [Add] button.
| 
 
Section select type 
 | 
 
Specify the method for specifying the section. 
 | 
| 
 
Default 
 | 
 
Section name 
 | 
| 
 
Modifying 
 | 
 
Select from the drop-down list. 
 | 
| 
 
Available values 
 | 
 
Section name 
 | 
 
Specifies the range by the section name. 
 | 
| 
 
Start and end address 
 | 
 
Specifies the range by the start and end address. 
 | 
| 
 
Section name 
 | 
 
Specify the section name.  
Note that this item appears only when [Section select type] is set to [Section name]. 
 | 
| 
 
Modifying 
 | 
 
Directly enter from the keyboard.  
 | 
| 
 
Start address 
 | 
 
Specify the start address.  
Note that this item appears only when [Start and end address] is set to [Section name]. 
 | 
| 
 
Modifying 
 | 
 
Directly enter from the keyboard.  
 | 
| 
 
End address 
 | 
 
Specify the end address.  
Note that this item appears only when [Start and end address] is set to [Section name]. 
 | 
| 
 
Modifying 
 | 
 
Directly enter from the keyboard.  
 | 
 
[Function buttons]
| 
 | 
 | 
| 
 
OK 
 | 
 
Finishes configuring the target sections, and closes this dialog box.  
 | 
| 
 
Cancel 
 | 
 
Cancels any changes to the target sections, and closes this dialog box.  
 | 
| 
 
Help 
 | 
 
Displays the help for this dialog box.  
 |