|
RS-CAN Module Setting dialog box [Full-spec emulator][E1][E20] |
This dialog box is used to make settings related to the entire RS-CAN module shown in the Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20].
This section describes the following.
On the Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20], click the [RS-CAN Module Setting...] button on the toolbar. |
Select the clock source for the RS-CAN module from the following drop-down list.
The actual frequency of the specified clock source appears at the bottom of the drop-down list.
Specify whether the timestamp function of the RS-CAN is to be used.
Specify whether the Data Length Code (DLC) checking function of the RS-CAN is to be used.
Specify whether the DLC replacement function of the RS-CAN is to be used.
This item is specifiable only when the DLC checking function is used.
|
Reflects the clock source, timestamp, DLC checking function, and DLC replacement function settings that were made in this dialog box to the [RS-CAN settings] area on the Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20]. |
|