This dialog box is used to set the serial format for the serial interface (IIC, IICA).
This section describes the following.
On the Serial window with the IIC serial interface, any one of the following:
|
Directly inputs the width at high level of the serial clock. |
||
|
Directly inputs the address of the slave which is to be the other party. |
||
|
Selects the pin for use in the input and output of a serial clock to the microcontroller from the drop-down list.Note |
||
|
Selects the pin for use in the input and output of serial data to the microcontroller from the drop-down list.Note |
||
|
Selects this item to repeat data transfer when the [Auto Send] or [Auto Receive] button in the Serial window has been clicked. |
||
|
Following transmission of the last data during automatic transmission, returns to the beginning of the data and performs automatic transmission. Following reception of the last data during automatic reception, returns to the beginning of the Wait time and performs automatic reception. |
||
|
Following transmission of the last data during automatic transmission, stops transmission. Following reception of the last data during automatic reception, stops reception. |
||
When the port pin to which a multiplexed pin function is assigned in the peripheral I/O redirection register is to be changed, select the pin in accord with the settings. If the selected pin does not correspond to the settings of the peripheral I/O redirection register, data will not be correctly sent and received in the Serial window. |
|
Selects the pin for use in the input and output of a serial clock to the microcontroller from the drop-down list.Note2 |
||
|
Selects the pin for use in the input and output of serial data to the microcontroller from the drop-down list.Note2 |
||
|
Selects this item to repeat data transfer when the [Auto Send] or [Auto Receive] button in the Serial window has been clicked. |
||
|
Following transmission of the last data during automatic transmission, returns to the beginning of the data and performs automatic transmission. Following reception of the last data during automatic reception, returns to the beginning of the Wait time and performs automatic reception. |
||
|
Following transmission of the last data during automatic transmission, stops transmission. Following reception of the last data during automatic reception, stops reception. |
||
These items are disabled when IIC is selected from the list of serial interface types in the Serial selection area. This is because there is no wait state and data are automatically received. |
When the port pin to which a multiplexed pin function is assigned in the peripheral I/O redirection register is to be changed, select the pin in accord with the settings. If the selected pin does not correspond to the settings of the peripheral I/O redirection register, data will not be correctly sent and received in the Serial window. |
(default)
(default)