| Parts Led Properties dialog box | 
This property dialog box is used to set or change the pin connection information of LED, which are one of the connection parts in the I/O Panel window. 
A pin-connected LED displays the information output from the simulator through lit/unlit display in the Simulation mode. 
There are two types of LED display styles, figure and bitmap. These styles can be changed on the [[Style] tab]. 
| 
Figure A.80 | Parts Led Properties Dialog Box: [LED Connection] Tab | 
| 
Figure A.81 | Parts Led Properties Dialog Box: [Style] Tab | 
 
This section describes the following.
[How to open]
On the I/O Panel window, any one of the following:
| 
- | Double-click a part object "LED". | 
| 
- | Select [Properties...] form the context menu on a part object "LED". | 
| 
- | Select a part object "LED", and then select [Properties...] form the [View] menu. | 
[[LED Connection] tab]
| 
(1) | Pin connection information setting area | 
| 
Label | 
This area is used to specify the part name. The part name input here is also displayed in the Parts List dialog box as the label. | 
| 
Pin Name | 
This area is used to specify the pin name to be connected (output pin). The connection pins can be specified either via direct input or through selection from the drop-down list. | 
| 
Active Level | 
The active state is selected with a option button, as follows: | 
| 
LOW | 
Sets the active level to LOW. | 
| 
HIGH | 
Sets the active level to HIGH (default).  | 
| 
Remark | For the pin names that can be specified, see the user's manual of the microcontroller that is used. | 
[[Style] tab]
| 
(1) | Style information setting area | 
| 
Figure | 
Select this option button to display the LED with the following specified figure. | 
| 
Shape | 
Select the figure shape. Two shapes can be selected: rectangle and ellipse.  | 
| 
shadow | 
Cannot be selected. | 
| 
Line | 
Specify and change the figure line, as follows. 
You can change the color of figure line by clicking the pull-down button.  | 
| 
Thickness | 
Specifies the line thickness.  
Specification is made either using a spin button or through direct input.  
A value from 1 to 100 can be specified.  | 
| 
Active | 
Specifies the color of the line during active display. | 
| 
Inactive | 
Specifies the color of the line during inactive display. | 
| 
Fill up | 
Specify and change the figure filling, as follows. 
You can change the color of figure filling by clicking the pull-down button.  | 
| 
Active | 
Specifies the fill color during active display. | 
| 
Inactive | 
Specifies the fill color during inactive display. | 
| 
Bitmap | 
Select this option button to display the LED with the following specified bitmap (default). | 
| 
Selection list | 
Select a bitmap to be used from the selection list.  
The selectable bitmaps appear in the selection list. | 
| 
[Add] button | 
Opens the Entry Bitmap dialog box below to add a new bitmap to the selection list.  
The bitmap file to be added can be specified either through file selection using the [...] button, or through direct input. | 
| 
[Delete] button | 
Deletes the currently selected bitmap from the selection list. 
Note that only the bitmap that have been added by user can be deleted. | 
This area displays the style of the LED currently being specified.
[Function buttons]
|  |  | 
| 
OK | 
Validates the settings and closes this dialog box. | 
| 
Cancel | 
Cancels the settings and closes this dialog box.  | 
| 
Apply | 
Cannot be selected. | 
| 
Help | 
Displays the help for this dialog box.  | 
[Operation]
In the Simulation mode, the output status (active/inactive) of the connected pins is displayed in real-time using two types of bitmaps or figures. 
| 
Figure A.82 | Connected Parts Display Example (LED) |