This function closes a project.
[Specification format]
project.Close(save = False)
|
[Argument(s)]
|
|
|
|
save
|
Specify whether to save all files being edited and a project.
True: Save all editing files and a project.
False: Do not save all editing files and a project (default).
|
[Return value]
If the project was closed successfully: True
If there was an error when closing the project: False
[Detailed description]
- | This function closes a currently opened project. |
- | If save is set to "True", then all files being edited and a project are saved. |
[Example of use]
>>>project.Close()
True
>>>
|