This function removes a file from the active project.
[Specification format]
project.File.Remove(fileName)
|
[Argument(s)]
|
|
|
|
fileName
|
Specify the full path of the file to be removed from the active project.
When specifying multiple files, specify in the format ["file1", "file2"].
|
[Return value]
If a file was removed from the active project successfully: True
If there was an error when a file was removed from the active project: False
[Detailed description]
- | This function removes the file specified in fileName from the active project. |
- | The file is not deleted. |
[Example of use]
>>>project.File.Remove("C:/project/sample/src/test.c")
True
>>>project.File.Remove(["C:/project/sample/src/test1.c", "C:/project/sample/src/test2.c"])
True
|