| Add Folder and File dialog box | 
This dialog box is used to add existing files and folder hierarchies to the project.
The folder is added as a category.
| 
Figure A.10 | Add Folder and File Dialog Box | 
 
The following items are explained here.
[How to open]
[Description of each area]
Select the type of the file to be added to the project.
You can select multiple file types by left clicking while holding down the [Ctrl] or [Shift] key.
If nothing is selected, it is assumed that all types are selected.
| 
(2) | [Subfolder level to search] area | 
Directly enter the number of levels of the subfolder to be added to the project.
"1" is displayed by default.
| 
Remark | Up to 10 (decimal number) can be specified.When the input violates any restriction, the following messages will be shown in the tooltip.
 | 
|  |  | 
| 
Fewer than 0 or more than 10 values cannot be specified. | 
More than 10 subfolder levels have been specified. | 
| 
Specify in decimal. | 
A number in other than decimal or a string has been specified. | 
| 
Caution | The name of a network path cannot be used. Assign the name of a path on a drive. | 
[Function buttons]
|  |  | 
| 
OK | 
Adds the folder that was dragged and dropped and the files in that folder to the project.  And then closes this dialog box. | 
| 
Cancel | 
Does not add the folder and files, and then closes this dialog box. | 
| 
Help | 
Displays the help of this dialog box. |