Everything
 

User Setting dialog box


This dialog box allows you to customize toolbars and menus displayed in the Main window.

When this dialog box is open, any button on a toolbar or any menu item in a menu bar currently displayed in the Main window can be dragged and dropped to the desired position to change the sequence of buttons or menu items or perform button/menu item deletion.

Caution

While this dialog box is open, you cannot use functions of toolbars/menus.
You can use these functions as usual after you close this dialog box.

Figure A.58

User Setting Dialog Box

 

The following items are explained here.

[How to open]

-

From the [Tool] menu, select [Customize...].

[Description of each area]

(1)

Tab selection area

Tab selection allows you to switch between the customization targets.

This dialog box has the following tabs:

(2)

Customization area

You can set detailed customization conditions.

For details of displayed items/setting method, see the description of each tab.

[Function buttons]

Button

Function

Keyboard...

Opens the Customize Keyboard dialog box to assign customized items to keys on the keyboard.

Close

Cancels the toolbar/menu customization setting and closes this dialog box.