Everything
 

One Point Advice dialog box


This dialog box is used to display tips for using CS+.

Figure A.69

One Point Advice Dialog Box

 

The following items are explained here.

[How to open]

-

From the [Help] menu, select [One Point Advice...].

-

Automatically opens at CS+ startup when [Do not show this dialog box at startup] is unchecked.

[Description of each area]

(1)

Tips display Area

Tips for using CS+ are randomly shown (edit not allowed).

(2)

Page feed area

The current page number in this dialog box and the buttons for page feed are shown.

Button

Function

Back

One previous page is shown.

The button is disabled when the first page is shown.

Next

One next page is shown.

The button is disabled when the last page is shown.

(3)

[Do not show this dialog box at startup]

This configuration is saved as the one for the active user.

 

Does not open this dialog box automatically at startup.

 

Opens this dialog box automatically at startup when Main window appears (default).

Remark

This property can also be set from the Option dialog box, under the [General - Startup and Exit] category.

[Function buttons]

Button

Function

OK

Closes this dialog box.

Help

Displays the help of this dialog box.