| 
 Plug-in Manager dialog box 
 | 
This dialog box is used to set the plug-ins to be read in when this product is started.
Caution  | The settings in this dialog box are effective from the next time this product is started.  | 
 
Figure A.55  | Plug-in Manager Dialog Box  | 
 
 
The following items are explained here.
[How to open]
-  | From the [Tool] menu, select [Plug-in Setting...].  | 
 
[Description of each area]
By selecting a tab, the plug-ins displayed in the plug-in list area are switched.
This dialog box has the following tabs:
Select the plug-ins read when this product is started with check boxes.
For details of displayed items/setting method, see the description of each tab.
Remark  | You can select all check boxes or clear them by clicking buttons displayed on the upper left of this area.  | 
 
| 
 
 
  
 | 
 
Selects all check boxes. 
 | 
| 
 
 
  
 | 
 
Clears all check boxes. 
 | 
| 
 
 
  
 | 
 
Toggles all check boxes. 
 | 
 
[Function buttons]
| 
 | 
 | 
| 
 
OK 
 | 
 
Applies all setting and closes this dialog box. 
 | 
| 
 
Cancel 
 | 
 
Cancels the designated condition and closes the dialog box. 
 | 
| 
 
Help 
 | 
 
Displays the help of this dialog box. 
 |