< Compile Options / Dependency File Output Specification Options >
[Format]
Processing continues without analyzing dependencies. A header file dependency file is not output.
[Description]
- | This option analyzes only the header file dependencies for the input file, and then outputs the results to a file. |
- | The output file name is the same as the input file name with the extension replaced by “dep”. |
- | You can specify the file name to be output by using the -MF option. |
[Example]
ccrx test.c -isa=rxv3 -MM
|
<test1.h>
#include "test2.h"
|
<test.c>
#include <stdio.h>
#include "test1.h"
|
test.obj: test.c
test.obj: test1.h
test.obj: test2.h
|
Note 1. | The output might include a path. |
Note 2. | The example shows only some of the files in the output file. The actual output file contains all files with dependencies. |
[Remarks]
- | The following two types of header files are output: |
- | File included by specifying the -preinclude option |
- | File included by specifying #include "file-name" |
- | Note that the file included by specifying #include <file-name> is not output. |