Everything

-MD [V3.08.00 or later]


< Compile Options / Dependency File Output Specification Options >

[Format]

-MD

 

-

[Default]

Dependencies are not analyzed. A header file dependency file is not output.

[Description]

-

This option analyzes the header file dependencies for the input file, and then outputs the results to a file.
Compilation processing is also performed.

-

The output file name is the same as the input file name with the extension replaced by “dep”.

-

You can specify the output file name by specifying this option together with the -MF option.

-

This option is invalid if the -output=dep or -MM option is also specified.

[Remarks]

-

For details about output files, see the description of the -output option.